Other Parts Discussed in Thread: TPSM63606, LM61460
Hi Sir,
My self i'm Sandeep,
I'm working as a Lead hardware design engineer in Elogic Engineering Services Pvt Ltd, Hyderabad, India.
I'm looking for Switching Regulator and LDO for my new project IoT gateway application,
I found this LMR51450 Regulator for 12V (max-36V) to 5V conversion@ 5A-6A current load,
Can i use this Regulator for IoT application and also if possible can you please suggest required parts for this application..
My Requirements are
1. Switching Regulator - Input: 9V to 36V -> Output: 5V and Current Out: 5A-6A max,
2. LDO - Input: 5V -> Output: 3.8V and Current Out: 2A-3A max,
3. LDO - Input: 5V -> Output: 3.3V and Current Out: 2A-3A max,
4. LDO - Input: 5V/3.3V -> Output: 1.8V and Current Out: 1A max