1.There is a scenario: The communication is interrupted abnormally, and the BQ76952 triggers the host watchdog fault. In this case, can the shutdown be enabled?
Single undervoltage Total undervoltage shutdown is not considered
2.There is another problem After the balance was turned on, I tried to turn off the balance, and waited for 1S to read the cell voltage, and found that Cell16 would still be low. Will we equalize the shutdown time very slow? I see the sampling time is around 3ms. Wait for 1S to read the voltage should be normal, right?