Other Parts Discussed in Thread: BQ25723, TPS65987, TPS65987D
Hi engineers:
I have built a fast charging circuit using TPS65987DDH + BQ25723, now it charges properly when negotiating 15V input using PD adapter; it does not charge at 20V input.
The charging voltage of the battery used is 8.4V, the PD adapter supports a maximum 65W output, and ADCIN1 DIV=0.91
The following problems were found during use:
1, When charging using 15V input, charging is only possible if the PD adapter is plugged in first to allow the TPS65987DDH to load the firmware image, and then the battery is connected. How do I modify the configuration so that I can connect the battery first and then the PD adapter for normal charging?
2、After starting charging according to question 1, the battery will stop charging in about 2~3 minutes (the watchdog of BQ25723 has been turned off). At this time, I quickly unplugged the PD adapter once again to continue charging until the battery is full. How to solve this problem and what is the cause of the problem?
3, at the same time also found in the use of PD negotiation 20V input BQ25723 can not be normal for battery charging, but 15V input can be normal according to the description of the problem 1 charging, charging set to 8.4V/3.5A. 20V input regardless of the setting of the charging current for 3.5A or 5A can not be charged at this time to test the BQ25723's VDDA = 6.069V, VSYS = 6.69V are normal.
The following files are the TPS65987DDH firmware and circuit diagrams that I used:
PD sink 15V:
PD sink 20V (BQ25723 not charging):
Circuit diagram:
I would appreciate any help from experts to solve the above problem!
Thanks
Johnsin Tao