Hi All,
I have a question about the BQ51050B.
I am using BQ51050B to charge lithium battery 2000mA battery.
I know max charging current of BQ51050B is 1.5A. and I want to charge the battery at 1.2A.
So, I set below.
R1 : 62ohm
RFOD : 200 ohm
RILIM : 262 ohm
Ibulk = 314 / 262 = 1.2 A
However, when I measured the battery charging current, it was measured at 800mA.
Charging current is moved from 800mA to 0A. is it ok?

And how can I make it charge at 1.2A?
Additionally, I confirmed that wireless TX IC transmits at 9V 900mA, and TX coil inductance is 9uH, RX coil inductance is 8 uH.
Refer to below schematic