Team,
I want to check with you about 2 questions for my customer. Thanks.
1. For the spec as below, when VSNS voltage is about VSNS, TMR1, the Timer will start counting. the D/S only indicates the typical and min value, we want to check the max value. Is it possible that when VSNS voltage is higher than 2.5mV but the timer doesn't start counting.
2. Is there a distribution data of the VSNS to trigger the timer? They need to do the tolerance analyze.
Regards,
QIang