Hello experts,
About BQ756506-Q1, when we use GPIO inputs for thermistor connections for temperature measurements like below:
I have two questions and need your help.
1、BQ main ADC Effective number of bits is 16bit ,but GPIO resolution (Main & AUX ADC) is 152.59 μV/LSB.
From my side, for a 16bit ADC powered by 5V supply, the resolution should be 5V/(216-1)=76.3 μV/LSB. How to understand this difference?
2、What's the meaning of “VACC_MAIN_GPIO_RATIO” ? Does this parameter include the error of TSREF? As we know, if we want to calculate the accuracy of NTC circuit, we need to take both ADC Sampling error(ADC self) and supply error(TSREF) into consideration.