This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: need clarification on the output capacitor usage

Part Number: TPS1663

Hello Team,

We are using TPS1663 IC for our application and which is 48V application.

Now we have used two 100uF capacitors at output but the capacitor are colliding with the mechanical components. now we have the only option to reduce the capacitor size.

So we want to understand the below mentioned,

what is the use of output capacitor?

minimum required value of capacitor to be used at output side ?

Can we use only one capacitor or two is required?

Eval kit has two capacitor 1uF and 1000uF , do we really need this high value capacitors?