This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LV3842: New device recommend

Part Number: LV3842
Other Parts Discussed in Thread: LMZM23600

Hi team,

Could you help recommend new device?

Requirements: The function is similar to LV3842 and contains an inductor IC

input voltage DC 4V~24V,

Output voltage 3.3V

Load current 40mA or more

Low ripple

Keep the size small.

Thanks

Lillian