Other Parts Discussed in Thread: TPS923655, TPS922052, TPS922053, LM5177
I have the following parameters:
- VIN_MIN: 12V
- VIN_MAX:48V
- WLED Vf max of 18.5V
- Iled_max: 1.4A
- Analog dimming input.
It looks like the TPS923653 family of parts would be suitable here. Is there anything I should be aware of when using these parts in the buck/boost configuration? It looks like the evaluation kit only comes in the boost configuration. Are there any other parts here with dev kits that would work here that I should consider?
I will go through the detailed design procedure in the datasheet for the TPS923653 in the meantime but wanted to ask here.
Thanks!