Other Parts Discussed in Thread: TPS7A92
Team,
Can you please suggest an LDO with single channel and same specs as TPS7A89?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Venkat,
The closest we have is TPS7A92 for a single-channel low-noise 2A LDO.
TPS7A92 | TPS7A89 | |
Iout(Max)(A) | 2 | 2 |
Vin(Max)(V) | 6.5 | 6.5 |
Vin(Min)(V) | 1.4 | 1.4 |
Vout(Max)(V) | 5.2 | 5.2 |
Vout(Min)(V) | 0.8 | 0.8 |
Fixed output options(V) | ADJ | ADJ |
PSRR @ 100 KHz(dB) |
48 | 35 |
Noise(uVrms) | 4.7 | 3.8 |
Accuracy(%) | 1 | 1 |
Dropout voltage (Vdo)(Typ)(mV) |
260 | 260 |
Iq(Typ) (mA) |
2.1 | 2.1 |
Output capacitor type | Ceramic | Ceramic |
Thermal resistance θJA(°C/W) |
57 | 33 |
Operating temperature range(C) |
-40 to 125 | -40 to 125 |
Package size: mm2 | 6 mm2: 2.5 x 2.5 (SON|10) | 16 mm2: 4 x 4 (QFN|20) |
Regards,
Andres