This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI service team,
I have encountered one issue at UCD90160A PMBALERT_N pin (already pull-up to 3V SEQ VCC with 4.7K resistor) abnormal status (check below figure1) when power on system.
Can you help to check the reason why this pin is asserted even if power sequence is normally operated in the beginning (check below figure2)?
Thanks a lot.
Figure1:
Figure2:
Best Regards,
Paul Lei
Hi Yihe,
I noticed the results you mentioned are related I2C communication.
All rails are normally operated, there is only communication problem in the beginning, and I need to clear logged faults (figure1) to de-assert "PMBALERT_N" from L to H level (figure2).
(1) Is there any default I2C/SMBus (like congenital defects) communication problem when system boot up in the beginning ?
(2) How can I prevent from this kind of CML fault logs in UCD90160A in the beginning when rails are all ok ?
Thanks a lot.
Figure1:
Figure2:
Best Regards,
Paul Lei
Hi Yihe,
1. However, we have same design in other components with ALERT_N signal, SDA/SCL are all pulled-up to P3V3 which is the same voltage source to UCD90160A, and they won't assert ALERT_N signal to L, is there any other design requirements (HW / FW) in UCD90160A I haven't noticed ?
2. OK, got it, if we have this default assertion value, host can issue clear status (0x03h) command to reset this ALERT_N to H.
Thanks.
Best Regards,
Paul Lei
Hi Yihe,
For debugging of software, you mean it's to fix the configuration file in UCD90160(A) or the FW setup on my system.
However, I don't connect any host on my system in the beginning, but it still occurs CML fault in logs and causes ALERT_N pin assertion.
Thanks.
Best Regards,
Paul Lei
HI
I mean your host i2C software.
Please clarify what kind of CML fault. there are many faults embedded in the CML.
if you do not have a host, i won't expect any I2C communication on the bus. have you probed the SCL/SDA?
Regards
Yihe
Hi Yihe,
Can you talk more about 03h REG, clear fault command ?
I have seen some descriptions in datasheet (slua815b), UCD90160(A) doesn't support SMBALERT_N MASK function.
Can you help to check with your EVBoard for this alert pin (SMBALERT_N) status after powering up ?
Thanks.
Best Regards,
Paul Lei
Hi Yihe,
Got it and thanks.
I'll try to investigate other devices on same I2C bus path which might affect UCD90160(A).
One thing about fault I want to confirm again, when fault is cleared by 03h (clear fault command) to UCD90160(A), it won't let device restart, right ?
It should be cycled UCD90160(A) power supply or applied with retry mode to restart rails again, right ?
Thanks.
Best Regards,
Paul Lei