Other Parts Discussed in Thread: BQ27542-G1, BQSTUDIO
Hi
The customer test with BQ27542-G1. battery 4000mAh (3.8V). During the client system test, it was found that RM/FCC increased. The reason for the change and update mechanism need to be explained.
According to the customer's method, use the power supply and load to simulate 500mA charging to 80% and then use 8mA to discharge to simulate the system sleep state. Please check the log data. You can see that the FCC has a slight rebound after charging as reported by the customer. Could you please explain the FCC update mechanism?
565786-0.5A charge 8mA discharge.log
Waiting for your reply.
Thanks
Star