Hi
OV pin can be used as an Enable/ (active low eable).
Is it enough to just pull it to Low? need to add additional components? In the OV pin?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gareth,
Welcome to E2E!
Whenever voltage at OV pin is greater than 0.6V, it forces the MOSFETs to turn off. Hence any signal greater than 0.6V is enough and additional components are not required.
Regards,
Shiven Dhir