This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5064: How to add Soft start?

Part Number: LM5064
Other Parts Discussed in Thread: INA226, TPS23521

There is a training video that explains how to use the TI LM5064 calculator tool.

However the tool in the video must be a different version than the one I recently downloaded because it shows an additional soft start feature that mine does not have, to slow the inrush cycle.

My application is -48V @ 50A with 7000uF capacitance and it would be helpful if I can slow down / lower the inrush cycle / current, and not have to also slow the Timer function. 

There is no SS feature / pin on the LM5064 so I would have to design something around it to accomplish this (and I'm not sure it is possible / practical). 

Is there a suggested way to do this?