I am interested in using a high side gate driver (ex. UCC27714) with an N channel MOSFET to act like an electronic switch for a high voltage operation. I've researched a bit about high side gate drivers and noticed that they have a draw back in continuous operation cases. My case is the following:
- Source a 150V and 2A (300W) to charge a capacitive load
- The capacitive load needs about 15 to 20 seconds to fully charge (the N MOS would need to remain active for this time)
- Power source is connected to the Drain
- Capacitive load is connected to the Source
Would the UCC27714 gate driver work in this case?
Is there another gate driver that would be better recommended?
Would I need to use some sort of PWM to make this switch work? (I am not converting any voltage, just charging a capacitor and using the MOSFET as a switch)
Would I need to use a bootstrap capacitor and diode for this design?
Thank you,
Alex