This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H4010-SEP: Soft Start SET

Part Number: TPS7H4010-SEP

Hi, I am using this regulator to provide power rails (a 3.3V and a 1.8V)  for a microcontroller (Microchip SAMRH71) however I noticed in the SEE report that there is a Single Event Transient associated with the soft start circuit that turns the output off and then on with the internal 6ms soft start. This would power cycle the uC which is not acceptable for my application. Is there a possible workaround to this issue? 

Thank you