Hello,
We have a SEPIC design including the LM3481-Q1 controller.
According to the datasheet, Cin should be above 100uF.
However, the Powerbench suggests Cin to be tantalum 4.7uF.
The questions are:
1) Who should I follow, the datasheet or the Powerbench design?
2) 100uF tantalum or aluminum capacitors for automotive applications are not recommended. However, the LM3481-Q1 controller is for the automotive industry. Which capacitor do you recommend using as Cin in automotive applications? Is it, for example 4*22uF ceramic ones?
Awaiting your reply.