This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92692-Q1: TPS92692-Q1

Part Number: TPS92692-Q1

 am using PSPICE in Cadence Allegro 17.4. An error occurs in the simulation. 

I using olb file of TPS92692-Q1 Boost and Buck Boost PSpice Transient Model (Rev. A)   of   TPS92692-Q1 data sheet, product information and support | TI.com

What is the cause and solution to this error?



--------------- INFO(ORPROBE-3209): Simulation Profile: SCHEMATIC1-TPS92962_Q1_Simple_Circuit ---------------
INFO(ORPROBE-3183): Simulation running...
** Profile: "SCHEMATIC1-TPS92962_Q1_Simple_Circuit" [ d:\pspice\2024\ldm\inrush_current\bmw_g65_hl_jp\b121_hl_ldm_drl\tps92692_q1_s
Reading and checking circuit
ERROR(ORPSIM-16505): Missing value
Circuit has errors ... run aborted
See output file for details
INFO(ORPROBE-3188): Simulation aborted


  • Hello,

    I ran the simulation and did not get that error.  If you have changed the schematic then the error is with something you you've done and you will need to figure that out.  It's most likely some component you have added and do not have a value for it.

    Thanks Tuan