Part Number: LP5860
Hi team,
On the evaluation board, when the anti-ghost lighting function is turned on, a reverse voltage exceeding the absolute rating is observed in the LEDs.
This is probably a natural phenomenon due to the anti-ghosting mechanism, but there is no mention of this in the datasheet.
The LEDs mounted on EVMs have an absolute reverse voltage rating of 5V, but there are many LED manufacturers that have deprecated this rating rather than the numerical value.
I would like to know how it is determined that the De-ghost function does not affect the LEDs in this regard.
Sincerely,
Ryu.