Hello team,
Can I use TPS2596 like a high side switch on the diagram below?
The app note: Driving PWM Loads with TI High-Side Switches says high side switch can be used as high side protection for PWM generator (Low side Driver).
The PWM frequency would be 150kHz, so the load for TPS2596 would be 150kHz pulse with 200mA max.
Also, what are the general differences between efuse and high side switch? How do you chose to use either one of them in different conditions?
Best Regards,
Kei Kuwahara