This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65219: TPS6521908 PIN setting

Part Number: TPS65219

Hi team,

Could you help check how to set the MODE/STBY   MODE/RESET   VSEL_SD/VSEL_DDE   PIN?

How to connect these PIN?

LPDDR =1.1V

Thanks

Lillian

  • Hi Lillian,

    The pin connections depend on what you want to accomplish and how you have your registers programmed.

    The datasheet describes how each pin should be configured and the functional result of each configuration.

    Starting in Section 7.3.8, there are definitions for each MFP (Multi-function pin). I would recommend looking at Table 7-3 and Table 7-4 as a reference.

    The tables in the TPS6521908 Technical Reference Manual also show the functional result of each MFP configuration.

    If you have a question about a specific configuration or setting, let us know.

    Regards,

    James