Other Parts Discussed in Thread: TPS23861, , LM5156
Hey Boost Regulator team,
I have a customer evaluating the LM5156H for a new project where they need to implement an isolated 24V to 48V boost circuit in order to power the PoE PSE system which uses the TPS23861. The PoE power requirement is 30W per port so we need a boost circuit that can support ~100W total. The LM5156HEVM-FLY dev kit and design seems to support 5V out at 4A and we're hoping the circuit can be modified to fit the requirements for this application.
A couple questions on our side:
- Can the LM5156HEVM-FLY Schematic depicted in Figure 6-1 of the EVM design guide be used to achieve the isolation requirements for the PSE controller that was described above?
- Is the isolation transformer from the LM5156HEVM-FLY BOM capable of handling 100W?
- Are there any other constraints or limitations we should be aware of going into this power tree design?
Let us know if anything needs further clarification!
Best regards,
Matt Calvo