Other Parts Discussed in Thread: TPS54620
Hi Expert,
I would like to know if I use I2C set TPS62871 VREF as 0.5V, VOSNS and GOSNS connect to remote sense output voltage and GND accordingly, no matter VOSNS pin voltage higher or lower than 0.5V then the TPS62871 will regulate VOSNS voltage to 0.5V by PWM correct?
Actually I would like to know is if TPS62871 VOSNS pin voltage higher or lower than VREF then Duty will lower or higher to make VOSNS voltage keep same as VREF, because in TPS62871 block diagram it’s a little bit different compared with normal POL, normal POL it will be a error amp and + side will be VREF but TPS62871 not.
Thanks.
Best Regards,
Roy