Other Parts Discussed in Thread: BQ25720
Hi Team,
The charging current of the customer project needs up to 12A. The datasheet of BQ25710 shown that when it is 10mohm, the maximum charging current can supported 8.128A. Can BQ25710 change the charging precision resistor to 5mohm to support the charging current to 16A?
Can you help me confirm if this is possible? If feasible, how to design the layout?
Many thanks~