Other Parts Discussed in Thread: TPS51220A,
Hello WV support team,
My customer uses TPS51220A a lot, however, which TPS51220A is old part and we are moving to new solutions.
We will suggest LM5143, but the 100% duty cycle requirement is the need for customer's request.
The input voltage will be 12V to 24V for the system and the output is 12V here.
Thus, the 100% duty requirement will happen at the 12V condition for them.
According to the minimum off time, the LM5143 is 80ns comparing to the TPS51220A's 160ns, which means when operating at low fsw, the duty is possible to reach 99% at 100kHz, and 97% at 300kHz.
We want to make sure at this condition, the 12V-to-12V scenario is able to reach within ±5% output voltage requirement?
Because TPS51220A's datasheet states that it's able to reach 99%, and based on the data, LM5143 is more well-behaved, so it seems no problem for this application, right?
Best Regards,
Dave