Part Number: UCC21530
Other Parts Discussed in Thread: TIDA-00366,
I was referring to TIDA-00366 document. I assume that the DC voltage generated would be in the order of 400V if the input supply is 230V,50Hz. Whether the DC voltage is sufficient for the circuitry to generate 0 to 320V three phase output voltage up to 250V and it can drive 3 phase motor/3-phase transformer