Hi all. I have a customer board with an onboard charger circuit for a 12V lead acid battery inpu which I would like to protect against reverse polarity.
The LM7310 mentions reverse polarity protection, but specifcially 'input reverse polarity protection'
I assume this is explicitly mentioned, but I do not see output reverse polarity mentioned in the datasheet.
So the system would be: charger > LM7310 > battery > LM7310 > system
The second chip would protect the system against reverse polarity for sure.
However I am worried about a reverse polarity event damaging the output of the first LM7310.
Would this setup work and/or are there better ways of doing it?