This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: disable SCDL PF trigger

Part Number: BQ76952

I'm using this chip in a slightly none standard way, where we have an emergency direct connect to the battery that bypasses the fets. this was done because even if the battery is on fire this line cannot lose power till the very end, but when the fets are off and some current is pulled thru this bypass the SCDL PF triggers. is there a way to disable the SCDL from triggering a permanent fault?