Other Parts Discussed in Thread: CSD17577Q5A
Hi Ti Experts,
I’m trying to use LM5176 to boost a single 21700’s voltage to a constant 24V.
Referencing the below generated Webench design, a prototype board is already designed and built.
webench.ti.com/.../SDP.cgi
The worst case Vin is assumed to be 2.8V and a lipo battery’s voltage shall never exceed 4.2V. This particular design suggested that I will need a separate voltage source for Vbias to allow the below 4.2V input voltage to work. I somehow misunderstood the datasheet, thought Vbias was optional during designing, so all I did was to include Cbias and anticipate manual rework if needed.
Now after building the PCB, the circuit of course didn’t work with a 3.7V input, where Vin is below the 4.2V input baseline specified in the datasheet. Later, I was able to get the board to output ~24V with an input of 5V. Vin after a ~500mV diode drop still provides sufficient voltage for the IC to run without Bias. It makes sense that the circuit was not functional with a 3.7V battery after knowing that I’ll need external power to Bias pin to get low vin to work. I realized this is a config that will never work for the product I am developing for, as this power stage should be able to be activated without an external power supply.
I then tried to regenerate the design with the “Bias to Vout” option. Referencing the design, I simply reworked the board to have Vout connected to Bias. The circuit was not boosting. As I increased the input voltage to around 5V, the circuit was damaged, likely the SW1 and SW2 pins on the IC. I don’t think the switching FETs are damaged after taking them off and probing their Rds. Later I compared the two designs “Bias to Vout” vs “External Bias Source”, I realized that the switching FETs for “Bias to Vout” have significantly higher voltage rating than the ones for “External Bias Source”
So I think I have two main questions:
- Should the “Bias to Vout” config work for my application and design parameters of min Vin voltage being 2.8 from a single 21700 battery, given that my schematic will be referencing the generated Webench design correctly.
- Is the FETs with lower voltage rating the main reason why the IC was damaged during my rework? Otherwise I don’t have a theory of why my manual rework didn’t get IC to operate in PWM mode, while Bias is connected to the Vout rail.
Thank you very much for your time!