Have 12V being supplied at VIN from a power supply. J1 and J3 are open. No matter what ILIM setting I choose or whether there is a load or not VOUT1 is constantly at 3.8V and VOUT2 is constantly at about 5.8V, so it seems they are both clamped at their OV clamp values. Their FLT lines are sitting around 3.4V and the LEDs are not on. Could it be that these two parts are damaged? Or am I doing something wrong?