HI SIR
I Need a 10A output , could I use the LM76005 Parallel output?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Alex,
Not recommended, what are your VIN and VOUT requirements?
Thanks.
David.
Hello Alex,
What is your input voltage requirement? what is the input voltage range?
Thanks.
David.
Hello Alex,
This device is rated to 10A and can deliver 25V out at 10A, but will depend on load profile requirements, frequency selection, along with thermal management.
Hope this helps.
David.
Hello Alex,
You can use this device if you would like to. We also have a single output device that is in preproduction. Please see link below.
LM70880-Q1 data sheet, product information and support | TI.com
This device is rated to 8A continuous output current and can also be put in parallel.
You can also refer to application note below and implement the same scheme for the LM76005.
Configuring LM62460 for Dual-Phase Operation
Hope this helps.
David.