Hi,
1. May I know BQ25172 can use in 2S2P application? Or anything need to noticed?
2. For IC temperature calculate, can I using (Vin-Vout) * Iout = Pd?
Thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
1. May I know BQ25172 can use in 2S2P application? Or anything need to noticed?
2. For IC temperature calculate, can I using (Vin-Vout) * Iout = Pd?
Thanks!
Jeff
For IC temperature calculate, can I using (Vin-Vout) * Iout = Pd?
Yes this is correct.
May I know BQ25172 can use in 2S2P application? Or anything need to noticed?
It is best to check with the Battery Manufacture on this question they can also answer question on, cell balancing, rate of charge and temp for a 2S2P Pack.
From a BQ25172 standpoint it will see this configuration as a 2S1P for charging and would not be a problem. (update)