This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5023: LM5023

Part Number: LM5023


Hi,

I tried to design a flyback converter using lm5023 with following specifications,

Vin=500 - 750 V

Vout= 5V, 5A

But when I enter these parameters on webench power designer it shows design cannot be created due to some reasons. I was only able to simulate the design with minimum input voltage of 40V.Can the above mentioned part can meet my design specifications?