Other Parts Discussed in Thread: BQ25570, , BQ25504
Hi,
my end goal is building a USB C charger (for an eInk device) that is powered by a solar cell (ca 300 cm^2) in indoor lighting conditions.
The ouput power of the solar cell is about 10 mW under 1000 lux. I can manufacture the solar cell to deliver around V_MPP = 0.4 V and I_MPP = 25 mA (chinging with light intensity), but I can also connect several smaller solar cells in series and, therefore, increase the voltage and lower the current. The more cells I connect in series, the more power will be lost. So it is possible to reach 1.2 or 1.6 V (with 8 or 6 mA), but making a solar cell with 5 V will not be efficient.
For the USB charging, I need 5 V and 50 - 100 mA output for the device to charge properly. To reach these values I thought about charging up a supercapacitor with the solar cell and, once it is charged, the supercapacitor should be able to charge the eInk device for a short time, until the supercap falls below a certain voltage and needs to be charged again.
In the search for an IC, I found the series BQ255xx (BQ25504, BQ25505, BQ25570) and my question would be if you could recommend any of them (or also any other part of TI that I might have missed).
My thoughts so far: I liked the BQ25570 because it seems to have both parts (charging the supercap and charging the device) included, but my doubts are about the buck converter. As far as I understand it, a buck converter is a step-down converter. So this would mean that the voltage of the supercap would need to be higher than 5 V and most of the supercaps I saw are at 2.7 or 3 V. So this wouldn't work, correct?
That would leave me with the BQ25504 or BQ25505 and an additional boost converter. I don't see any advantage of the additional gate driver of the BQ25505 and I could see that the adjustable VBAT_UV of the BQ25504 could come in handy, so I tend towards the BQ25504. Do you agree with me? Can you recommend me a supercap and an appropriate boost converter that would make sense in my application?
Do I need anything else to make the system work?
The difference between a normal boost converter and the energy harvesting circuits is the MPP tracking?
Thank you very much for your help!