Hi,
I'm using a TPSM365R6FRDN in my project to convert 54V to 5V with a 150mA load on the output side (5V).
I designed it and tested and the output voltage is 5V and everything seems fine. The only problem is that the temperature is too high and around 85C.
I'm wondering if anyone can check this design and guide me on how I can solve the temperature rise issue.
Thanks