This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5121: LM5121:Iout_max

Part Number: LM5121

Hi,

Please tell me the current output rating (Iout_max) for the LM5121.

I couldn't read it from the datasheet.

Best Regards,Katsuyama

  • Hi Kansuke,

    thank you for using the E2E forum.

    The LM5121 is a controller - this means it has the MOSFET external.

    The max current is defined by the Power Stage (MOSFET and Inductor). As this are all external components the LM5121 does not limit the max current and therefore this parameter is not given in the datasheet.

    Best regards,

     Stefan