This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IIN_SCALE_MONITOR in Fusion Digital Power Designer

Hi,

How do I set IIN_SCALE_MONITOR in Fusion Digital Power Designer GUI?

Thanks,
Lukas

  • The parameter setting can be found on the Advanced Config tab on the Configure page in the Fusion Digital Power Designer GUI.

    If the tab is not visible in the version of the GUI that you are using then click on File --> Preferences and check the box for Show Advanced Editors and Featurs that are Normally Hidden in the window that opens and click OK.

    The parameter is set in ohms and would be the product of the current sense resistance and the gain of the amplifier which is feeding the result to the VIN/IIN multiplexer.

    The gain should be selected to prevent the maximum amplifier output voltage from exceeding the measurement capabilities of the 12-bit ADC (2.5V).