This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24230: BQ24230

Part Number: BQ24230

Dear Mr./Mrs.:

I could not find in the datasheet the termination current threshold for the bq24230. So, please, could you tell me the % of I charge current?

Thank you

  • Hello, 

    Thank you for reaching out via E2E. The % of charge current which is the termination current threshold will depend on the state of EN1 and EN2 pins. Below I have included the section of the datasheet where this is specified. For your reference it is located on page 10.

    If EN1 and EN2 are not both driven to GND then termination is approx. 10% of charge current. If both EN1 and EN2 are driven to GND then termination is approx. 3.3% of charge current.

    Best Regards,

    Garrett