Hello team,
My customer is asking about how to terminate unused pins.
Do you advise below unused pins?
Pin 6 : D+
Pin 7 : D-
Pin 12 : QON
Pin 16 : TS
Pin 24 : SDRV
Pin 25 : SYS
Best Regards,
Austin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Austin,
Please float D+, D-, QON. SDRV needs 1000pF capacitor to GND. SYS still needs its minimum capacitance after derating for applied voltage. If TS is floating, the charger reports a TS fault and prevents charge until the host processor sets IGNORE_TS bit =1. Or you can hardware disable the TS feature but using a 10k/10k resistor divider from REGN to TS to GND.
Regards,
Jeff