Part Number: BQ79718EVM-049
HI Team,
I am using BQ79718EVM-049 board for UV & OV protection and monitoring,
In my case I am using NFAULT as status of Fault indication. Following two conditions ware exist in the BQ79718EVM-049 board.
1) Fault condition: - When Cell Voltage < 1200mV then voltage between NFAULT & AVDD pin = -4.997V.
2) Heathy Condition: - Cell Voltage > 1200mV then voltage between NFAULT & AVDD pin = -0.289V.
Now, without resetting the board from GUI, I want to make NFAULT pin to be LOW, i.e. if cell voltage reaches to more than 1200mV then, the voltage between NFAULT & AVDD pin should become -0.2989V.
In overall I want to use auto resetting function in this board.