This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM8287A06: About CISPR rating

Part Number: TPSM8287A06
Other Parts Discussed in Thread: TPSM82866A, TPSM82813,

Hi team,

Does TPSM82876Axx and TPSM82813/4/6 comply with CISPR-11 class-B compliant standard like TPSM82866A?

Our customer is looking for module device that match below requirement.

・max load current: :6A

・Soft start time adjustable

・Power Good function

・protection : overcurrent, thermal shutdown

・comply with CISPR-11 class-B

I think match this requirement module device is this device. is there other recommend device?

Best regards,

teritama