This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65400: Inquiry on usage efficiency

Guru 11160 points
Part Number: TPS65400

Hello,

My customer has requested accurate efficiency information for the usage conditions below.

Please provide usage efficiency values for the five cases below.

CASE 1

Device Input Voltage Input Current Output Voltage Output Current Efficiency (%) Dissipated Power
(V) (A) (V) (A) 25 ℃ 80 ℃ (W)
TPS65400_C1 12 0.1 0.9 1     0.3
TPS65400_C2 12 0.16 1.2 1.3     0.34
TPS65400_C3 12 0.11 1.2 0.9     0.25
TPS65400_C4 12 0.25 1.8 1.4    

0.44

CASE 2

Device Input Voltage Input Current Output Voltage Output Current Efficiency (%) Dissipated Power
(V) (A) (V) (A) 25 ℃ 80 ℃ (W)
TPS65400_C1 12 0.17 0.925 1.75     0.46
TPS65400_C2 12 0.17 0.925 1.75     0.46
TPS65400_C3 12 0.24 1.8 1.35     0.46
TPS65400_C4 12 0.24 1.8 1.35     0.46

CASE 3

Device Input Voltage Input Current Output Voltage Output Current Efficiency (%) Dissipated Power
(V) (A) (V) (A) 25 ℃ 80 ℃ (W)
TPS65400_C1 12 0.15 1.2 1.2     0.36
TPS65400_C2 12 0.58 5.5 1.14     0.7
TPS65400_C3 12 0.26 5 0.5     0.63
TPS65400_C4 12 0.15 3.7 0.4     0.37

CASE 4

Device Input Voltage Input Current Output Voltage Output Current Efficiency (%) Dissipated Power
(V) (A) (V) (A) 25 ℃ 80 ℃ (W)
TPS65400_C1 12 0.17 0.925 1.75     0.46
TPS65400_C2 12 0.17 0.925 1.75     0.46
TPS65400_C3 12 0.24 1.8 1.35     0.46
TPS65400_C4 12 0.24 1.8 1.35     0.46

CASE 5

Device Input Voltage Input Current Output Voltage Output Current Efficiency (%) Dissipated Power
(V) (A) (V) (A) 25 ℃ 80 ℃ (W)
TPS65400_C1 12 0.15 1.2 1.2     0.36
TPS65400_C2 12 0.58 5.5 1.14     0.7
TPS65400_C3 12 0.26 5 0.5     0.63
TPS65400_C4 12 0.17 3.3 0.5     0.41

Thank you.

JH

  • Hi JH,

    Let me check and get back to you soon. Thanks!

    BRs

    Lucia

  • Hi JH,

    We have webench simulation tool to estimate the efficiency with different VIN, VOUT, load current and temp conditions. Please kindly change the condition and you can get the efficiency data.

    https://webench.ti.com/power-designer/switching-regulator/customize/111?VinMin=4.5&VinMax=18&O1V=1.8&O1I=4&base_pn=TPS65400&AppType=Dual&Flavor=Dual&op_TA=30&origin=pf_panel&lang_chosen=en-US&optfactor=3&Topology=Buck&flavor=Dual&VoltageOption=Dual&O2V=1.8&O2I=4

    Thanks!

    BRs

    Lucia