Part Number: TPS25750
I'm looking at using the TPS25750 for a project and it is everything I need, except I can't seem to find a way to dynamically disable the "source" capability. My device will be running on from its battery, but given a lower battery level, I want to disable the sourcing in order to preserve my device's operation. Is there a way to do that with a GPIO? I looked through the reference manual and played with the configuration GUI, but nothing stood out to me. I have a 3.3V logic signal available to determine if it should allow charging of another device, just not sure how utilize it (or if there is even a way). If not, is there a similar TI product with that ability?
Thanks!