Other Parts Discussed in Thread: TPS25750, TPS25751, BQ25756
Hi team,
Im working on a Proobe Of Concept to test the Power Delivery Chip working as a Source.
From the "TPS25750 Application Customization Tool" I've tried some settings but no one power up the VBUS with 5V.
How should I do configure the EVM and the software?
Let me clarify my settings:
Software from the GUI:
- 5V@3A power source provider
- Do not answer
- Do not answer
- Power Source as preferred role
- No USB data is being used
- Do not answer
- No Vendor ID
- No Product ID
- No battery Charger Configuration
Hardware:
- J1: 2-3 (Normal Operation)
- J2: Connect (Normal Operation)
- J4: Connected (Enable Flash Boot)
- J5: Disconnected
- PPHV Jumpers, connected to the P5V0 voltage (to power up this pad)
- SYS PWR (Test point): Connected to an external Power Supply at 20V
But the VBUS voltage is at 0V
The others Test Point (P3V3, P5V0, P12V0) are working fine.
Thanks