This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS799: Tps799

Part Number: TPS799

Im using TPS79928 fixed LDO which has 3.3V input and 1.8V enable. I'm getting output pulse of 540mV when the 3.3V input reaches 1.2V level but EN is still low. Could you please clarify the issue why the output is toggling to the intermediate 0.54v when there is no EN?