I have a circuit still in design which uses a TPS61222. CIN = 10uF, L = 10uH, COUT = 10U, with an additional 47mF supercapacitor on the output. The main purpose of this circuit is to charge a supercap for backup supply. There will be no load other than the supercap when the TPS61222 is first enabled. The supercap is 47mF with an ESR of 120 ohm.
There's two things I am worried about:
1) The datasheet doesn't mention a soft start time. I'm figuring since the supercap is 120 ohm I won't have a bad inrush problem.
2) stability - I know some DC DC converters compensation network can be dependent on the output capacitance. Will this be a problem with the TPS61222?