In our design we are using one external RC delay circuit for the power sequence application.
For discharging the capacitors on the RC filter we are planning to give one series resistor from capacitor to PG of the regulator TLV62585RW.
We are using this TLV62585RWT to convert the 5V to 0.75V. We are concentrating on the below red marked solutions for getting the PG pin as LOW state. We need to know the status of the PG pin and input voltage conditions on below two conditions(Marked in red) .

If the EN of the TLV62585RWT is in the LOW state, do we require any Vin voltage parameters to get the PG to the LOW state?