Hi
I'm using a board with TPS25750S connected with a host controller used to load the binary file.
The goal of the project is to use the tps25750 always in sink mode and switch in source mode only if the user decides to switch using the command SWSr. The starting configuration is Power Sink Only.
When I send the 4cc command "4SWSr" I read from register CMD1 0x08: 0x04 0x00 0x00 0x00 0x00 so the command has been executed but in the register DATA1 0x09 I read: 0x64 0x03, so the task has been rejected.
Where I'm wrong?
I attach the json and the i2c capture(Saleae).
/cfs-file/__key/communityserver-discussions-components-files/196/i2c_5F00_command_5F00_SWSr-and-json.zip