This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25883: Battery charger IC recommendation inquiry

Part Number: BQ25883
Other Parts Discussed in Thread: BQ25798

Hi, TI expert

A customer has an inquiry about battery charger IC recommendation.

It will use 2-Cell (approximately 3300mAh) and must support  Quick Charge Class A and up to 9V.

[spec]

- Cell chemistry (Li-ion / Li-Polymer / LiFePO4 / SuperCap) :  Li-Polymer

- 2-Cell (about 3300mAh) planned to be used

- Vin :  USB Voltage = 5V (9V when using Quick charging)

- Battery Charge voltage : Battery Nominal voltage 7.4V ~ Full charge 8.3 ~ 8.4V

- Charger Current (A) : 1.5A

- Control Interface (I2C / SMBus / Standalone) : I2C

- Control Topolgy (Boost / Buck / Buck-Boost/ Linear / Flash charger) : Boost

I found BQ25883 on ti.com, but Vin(max) is 6.2V.

Could you recommend a suitable part?

Also, I don't know if it's correct to check with Buck-Boost rather than Boost to find a part that meets the above spec.
Are there any TI parts that satisfy Quick Charge?

Please check. Thank you.