Other Parts Discussed in Thread: BQSTUDIO, BQ34Z100, , GPCCHEM
Hello TI team,
Technical information:
OS System: Windows 11
BQStudio 1.3.124
BQ34Z100EVM-Board
Fw Update (bq34z100_v2_02_00_31.exe)
After receiving my BQ34Z100EVM, it was initially recognized incorrectly.
I downloaded the latest firmware from your website.
I flashed the .srec (bq34z100_v2_02_00_31) with BQStudio via programming and moved the .bqz file manually into the folder C:\ti\BatteryManagementStudio\config.
Then I restarted BQStudio and now the selection was immediately skipped and the 0100_2_02 was preselected and started.
Now I performed a chemistry update (ChemUpdate1077.zip) and selected a suitable battery.
In this test, I selected a lithium thionyl chloride battery from the chemistry list.
It then transferred the update and indicated that it was successful, but also indicated that my bqz file was out of date.
Have I made a mistake? Do I need to download something else or has the bqz file in bq34z100_v2_02_00_31 not been updated yet?
It is also interesting that despite the correct chemistry ID selection, the visualization shows that the battery has only 6% or even 0%. the current is also rated 0.